Feedback_Kp

Index.Sub 2230.04H
Data Type Unsigned32
Access Read/Write
PDO Mappable No
Unit

--

Range

Unsigned32
Default Value

20000

Store Supported Yes
Description This value is used for Closed Loop feature and defines the position gain of PID’s regulator. The value has to be adjust to keep the position error (Feedback_Actual_Position_Error) inside the tolerance of application. The value can be set to 0 value when is necessary to have only a velocity controller and has not to be considered the position error.

Notes

A value too high could introduce motor’s vibration.